A program manager and packaging engineer supporting a long-lifecycle aerospace electronics platform were under pressure to reduce overall system cost without sacrificing electrical performance or reliability. Initial sourcing efforts focused on lowering substrate unit price using conventional PCB and thick-film technologies.
While component pricing appeared favorable, system integration began to reveal hidden cost drivers that extended far beyond the electronics themselves.
As the design matured, several cost multipliers emerged:
Over the program lifecycle, these secondary costs far outweighed the savings gained from lower-cost substrates. The team recognized that true affordability would come not from reducing unit price, but from reducing hand tuning, system complexity, and lifecycle risk.

Thin Film as a System Cost Optimization Platform
To address escalating program costs, the engineering team transitioned to a thin-film substrate platform designed to optimize total system economics.
Circuit Miniaturization Driving System Savings
High-dielectric materials, fine line geometries, and tight spacing enabled significant footprint reduction. Smaller circuits translated directly into reduced enclosure size, lighter housings, and more compact module packaging.
Thermal hardware scaled accordingly — smaller heat spreaders and reduced structural mass lowered both material and integration cost.
Functional Integration Reducing Assembly Complexity
Thin-film integration embedded resistors, capacitors, inductors, filters, couplers, and bias networks directly into the substrate. Eliminating discrete components reduced pick-and-place operations, solder joints, and inspection steps.
Fewer components also reduced failure points and long-term reliability risk.
Precision Eliminating Re-Spins and Tuning
Tight dimensional tolerances and repeatable electrical performance minimized unit-to-unit variation. Designs no longer required downstream RF tuning, or performance trimming after assembly.
This stability eliminated costly engineering re-spins and reduced schedule risk.
Process Stability Protecting Lifecycle Economics
Build-to-print execution locked materials, metallization stacks, and inspection criteria early in the program lifecycle. Statistical process control (SPC), documentation, and traceability ensured manufacturing consistency across prototype, qualification, and full production.
This stability protected programs from requalification costs triggered by supplier or process changes.
Targeted Use of Advanced Materials
Premium features — including filled vias, thick copper conductors, diamond heat spreaders, and AuSn eutectic metallization — were applied only where performance demanded them.
This targeted material strategy avoided over-engineering while still meeting electrical, thermal, and mechanical requirements.
Lower Total Program Cost Across the Lifecycle
After transitioning to the thin-film integration platform:
Despite higher unit substrate pricing, total program cost declined through removing of tuning necessity, reduced system material content, simplified assembly, and stabilized lifecycle manufacturing.
The platform enabled confident scaling from prototype builds to full-rate production using the same materials and processes.
[Engineering Takeaway]
“Unit price wasn’t driving our cost — system size, tuning, and requalification were. Thin film reduced enclosure size, eliminated re-spins, and stabilized production economics across the program lifecycle.”
— Aerospace Electronics Program Manager
This is our general contact form. If you have more specific questions or needs please select from the options below.