An optical packaging engineer developing next-generation transceivers for 400G, 800G, and beyond began encountering performance limitations that were not coming from the driver ICs or optical components themselves, but from the interconnect platform supporting them.
At these data rates, even very short electrical paths between the driver, TIA, and optical devices began to consume a significant portion of the system margin. As signals transitioned through bond pads, wire bonds, and routing structures, insertion loss increased and impedance discontinuities became more pronounced.
The impact was not isolated to a single failure mechanism. Instead, multiple small effects compounded:
As channel density increased and module size decreased, these effects became more difficult to manage. Designs required additional tuning and iteration to meet performance targets, and scaling from prototype to production introduced further variability.
The team realized that high-frequency performance was no longer limited by the active devices — it was limited by the precision and repeatability of the interconnect platform itself.

To address these limitations, the design was transitioned to a thin-film substrate platform engineered specifically for high-frequency signal integrity.
Highly defined, low-loss metallization replaced conventional conductor structures, reducing surface roughness effects and improving signal transmission at high speeds. Fine line geometries and thin substrates enabled tighter impedance control, allowing transmission paths to be designed with greater precision and consistency.
At the same time, the physical layout was optimized to shorten electrical paths. Precision pocketing and substrate features allowed the placement of devices closer together, reducing wire bond length and minimizing transition discontinuities.
Integrated thin-film passives were incorporated directly into the substrate, eliminating the need for discrete components and smoothing the signal path. This integration reduced parasitic effects while also freeing space within the module for higher channel density.
Because the platform was built using controlled, repeatable processes, electrical performance was consistent across channels and from unit to unit, reducing the need for post-assembly tuning.
With the thin-film platform in place, the transceiver design achieved stable high-frequency performance at advanced data rates:
By transforming the interconnect from a source of variability into a controlled, integrated structure, thin film enabled scalable, high-speed optical transceiver designs with consistent performance from prototype through production.
[Engineering Takeaway]
“At these data rates, the limitation wasn't the IC — it was everything between the IC and the optics. Thin film gave us the control we needed to maintain signal integrity across every channel.”
— Optical Transceiver Packaging Engineer
This is our general contact form. If you have more specific questions or needs please select from the options below.