Our customer was evaluating a solution for power electronics equipment that required the use of several DC-Link capacitors on the same PCB, while ensuring that the devices would support critical vibration profiles.
The products being considered for the application had a significantly high mass of around 100 g, and were attached to the PCB via four lead wires with 1.2 mm diameters. While testing these parts under severe vibration profiles, the customer reported broken lead wires.
The challenge was clear: how can such high mass parts withstand severe vibration profiles, while maintaining a similar footprint on the PCB?

Standard MKP1848 series DC-Link capacitors are supplied with lead wire diameters adjusted to the devices’ mass — from 0.8 mm for products with lead spacing of 27.5 mm, up to 1.2 mm for 52.5 mm lead spacing. On larger devices, four pins are also a standard feature. If properly clamped, this type of through-hole technology (THT) terminal is sufficient to withstand the vibration profiles described in general industry standards. However, to address our customer’s challenge, where the requirements exceeded the afore-mentioned standards, a more robust connection was needed to improve the capacitor’s grip on the PCB.
As a solution, the four lead wires of the DC-Link capacitors were replaced with two 1 mm tin-platted copper tabs. The perimeter of these tabs was over four times higher when compared with the original four pins, and section area was tripled. This led to a much higher contact area between the terminal and solder on the PCB, ruggedizing the connection as intended.
At the same time, all other electrical and robustness characteristics of the capacitors were validated and tested to demonstrate that the copper tab solution would not jeopardize either of them. The devices maintained their AEC-Q200 compliance and preserving THB characteristics for high robustness under high humidity products.


Prototypes were submitted to several vibration tests with different acceleration rates, frequencies, and amplitudes across the three axis. The testing showed significant improvement with the usage of tab terminals versus lead wires, and that our goal of offering the customer a DC-Link film capacitor that was able to support harsh vibration profiles was successfully accomplished.
The DC-Link film capacitors with tab terminals remain THT components. This allows the devices to be soldered to the PCB by conventional methods, preventing the need for any special processes to achieve a ruggedized fixation. The external dimensions of the capacitors are also maintained when compared with the original four-pin version, resulting in minimal design changes on the PCB. Only the holes and soldering pads needed to be changed to fit the new terminals.
Furthermore, this robust connection also improves ripple current capabilities through the capacitor, as the terminal section is improved while its resistivity drops, allowing for better power dissipation. This enhances the power density for the DC-Link capacitors.

Challenge
A customer’s design required a bank of polymer tantalum capacitors to achieve the necessary power level, but was restricted by a limited PCB area. However, the design offered available height that could be used if an appropriate solution could be found. It should be noted that apart from the specific length and width of a capacitor, and the footprint of the recommended solder pad dimensions, there are also “keep-out” areas on a PCB that can’t be used in order to prevent mechanical and electrical interference.
This is our general contact form. If you have more specific questions or needs please select from the options below.

Challenge
Installation and operating reliability are critical objectives for remote applications like wind turbines. With lost energy production and high maintenance costs being major issues for alternative energy applications, engineers continue to prioritize improvements to provide long term reliability to the utility companies that operate these wind farms. Due to their high energy levels, larger sized wind turbines have typically used multiple low voltage tubular AC capacitors in parallel, with a feed-through connection. The connection system for these capacitors is a small M5 screw that is susceptible to vibration forces. In addition, the security of the actual connection can be easily overlooked during the assembly process. Customers are also keen to avoid using oil-filled capacitors in the electronics system of the turbine, due to the potential damage caused in the event of a failure of the capacitor seal. However, the excellent performance of oil-filled capacitors has been an important factor in their application selection and usage.