ESTAspring Contacts for Improved Long Term Reliability in Wind Turbine Applications
Challenge
As the build-out of clean energy continues, the number of wind turbines deployed continues to increase. In fact, there are nearly 30 000 wind turbines installed in Germany alone (source: BWE Bundesverband WindEnergie e.V.).
Given their installation locations — including offshore and remote locations at high elevations — wind turbines are exposed to severe weather conditions, such as very high gusts and sustained winds. In addition, the very operation of wind turbines results in the entire system being subjected to extremely high and extended vibration forces. As a result, electrical connections of the high power components inside the system are potential “weak points.”
Adequate contact pressure over the long term and a low contact resistance for these component connection points is key. Power dissipation is converted into heat, which increases when current flows at the connection point. Because electrical connections are made of metal, the increase in resistance can generate temperatures of up to 600 °C at the defective connection point, depending on the magnitude of the contact resistance and of the current flowing (P = R x I²).
Power dissipation of 50 W or more is considered combustible, and processes that change the current load can further increase the already elevated contact resistance, because they subject the electrical connection to the expansion and contraction of pronounced thermal stress. This also results in a further degradation of the contact pressure, and the thermal stress usually causes further degradation in the conductivity of the conducting material, which leads to an even higher contact resistance. Maintaining a stable contact connection is therefore a very important requirement for these systems, in terms of safety and long term operating performance.
Given all of the above, catastrophic damage to wind turbines is quite possible. In fact, according to TÜV (German Technical Inspection Authority), it occurs around fifty times per year in Germany alone. One such potential failure mode is that the system catches fire. Once this happens, there is the possibility that a thirty meter long rotor blade will crash to the ground from a height of around one hundred meters. Fire departments are typically unable to extinguish flames due to the height of the wind turbine. Instead, they are forced to cordon off the area and attempt a controlled system burn until it exhausts the combustible material. In extreme cases, the towers can break and / or collapse, causing damage to other units or buildings in the immediate vicinity. The cost of a system fire, and replacing damaged equipment, can reach into the millions.

Solution
To solve this loose connection problem — especially in environments undergoing sustained vibration over the long term — Vishay developed the ESTAspring attachment system for the next generation of LVAC power capacitors. Instead of traditional screws, it utilizes lever-action spring contacts.
ESTAspring is a lever-lock spring connection for premade flexible conductors from 2.5 mm² to 25 mm² with bootlace ferrules. The maximum rectangular crimp geometry is 6.0 mm x 7.6 mm, and the spring is made of stainless steel that is corrosion-resistant. It uses a copper alloy conductor material that can handle currents of up to 90 A.
Vishay’s ESTAspring offers unprecedented ease-of-use. No tools or torque specifications are required for integrating these connections. The lever being closed assures a reliable contact with the necessary contact force and a simple visual check is all that is necessary for confirmation of a reliable connection.
Vishay’s PhMKP series capacitors — available with an oil filling or dry with a gas filling — are the first capacitors of this type available worldwide that offer the new ESTAspring safe connection technology. The devices feature rated voltages from 230 V to 1000 V, maximum reactive powers ranging from 2 kVAR to 37.1 kVAR, and maximum connection currents of up to 90 A.
Benefit
The always-constant contact force of ESTAspring assures a reliable connection over the entire service life of the capacitor and makes fires caused by defective contacts almost impossible. In addition to the improved reliability and safety for this harsh environment application, they provide a maintenance-free connection system for low voltage power factor improvement or harmonic filters in wind turbines, and other applications that experience high vibration environments.
UL/ULC has approved the polypropylene foil capacitors, in combination with ESTAspring, as a complete system.
Additional Case Studies

Avoiding a Complete Redesign After a Panel Potentiometer was Made Obsolete
Challenge
The customer approached Vishay when their existing panel potentiometer supplier discontinued production of a part used on an established and popular piece of equipment. To avoid a costly redesign, an existing panel potentiometer needed to be adapted to meet the customer’s electrical requirements. It would also have to fit the control panel insertion / retention envelope and existing markings, in addition to the PCB assembly attachment system.

DC-Link Capacitors With Tab Terminals For Harsh Vibration Profiles
Challenge
Our customer was evaluating a solution for power electronics equipment that required the use of several DC-Link capacitors on the same PCB, while ensuring that the devices would support critical vibration profiles. The products being considered for the application had a significantly high mass of around 100 g, and were attached to the PCB via four lead wires with 1.2 mm diameters. While testing these parts under severe vibration profiles, the customer reported broken lead wires. The challenge was clear: how can such high mass parts withstand severe vibration profiles, while maintaining a similar footprint on the PCB?

mmWave Loss and Unstable Performance in a Satellite Payload
Challenge
While developing a next‑generation Ka‑band and W‑band satellite payload for a low‑Earth‑orbit communications constellation, an RF systems engineer encountered an unexpected challenge. Although the team designed a GaN power amplifier and low‑noise receiver chain to operate above 80 GHz, system testing revealed significant performance degradation. The active devices met their specifications, but once the signal left the die, system performance collapsed: Insertion loss exceeded the link budget by 1.5 dB Parasitic inductance from wire bonds and interconnects distorted matching Board-to-board variation caused gain and phase inconsistencies across flight units Commercial passive components were too large and introduced resonances above 70 GHz The design relied on an advanced organic PCB with thick‑film passives and LTCC modules. Despite extensive tuning and redesign cycles, performance drifted from build to build, introducing unacceptable risk to schedule and qualification.
Have questions? We can help.
This is our general contact form. If you have more specific questions or needs please select from the options below.